cancel
Showing results for 
Search instead for 
Did you mean: 

Touchgfx files with C only!

Krautermann
Senior II

Every project generated from TouchGFX Designer is based on C++ (file .cpp). Is there a possibility to have project generated from TouchGFX Designer based on C only (file .c)?

Also are there any examples from TouchGFX Designer where the codes are in C?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

TouchGFX is completely based on C++, so it is not possible to generate pure C code.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

TouchGFX is completely based on C++, so it is not possible to generate pure C code.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.