User Activity

I want to implement a bare bones TouchGFX bootloader application that provides text based feedback for status & %programmed. The idea is for the bootloader to be in FLASH sector0 and for it to be able to program a more complex TouchGFX based applicat...
I want to communicate directly with a full speed CDC device from my STM32F769 running in USB host mode but I only have a high speed OTG USB port available. From example code for other STM32 devices it appears this is possible but can anyone confirm t...
I want to use the FLASH bank-swap feature of the STM32H753 for custom firmware updates. I have no problem erasing and programming FLASH bank 2 when running from bank 1 but I get a double bus fault when attepting to erase a sector in bank 1 when runni...
I'm running PC-Lint as an external tool with the results going an output console. I'd like to be able to double click on a PC-Lint error message in the console and have the appropriate source file / line displayed as per compiler errors. I have PC-Li...
Hi,I'm debugging a STM32F765 application using STM32CubeIDE v1.3.1 with ST-Link/V3 debug adapter via OpenOCD.The Memory window shows a gap of 800 RAM bytes in a valid RAM area (see picture below). Any idea what can cause this ?ThanksDave
Kudos from