STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Writting text with Unicode::fromUTF8 bug

Hi,I haver two text areas AAA and BBB both with wildcard buffer to write to. When use the funcion Unicode::fromUTF8 to write some text and the text is larger than the buffer the values of the two text areas are concatenated and writted on the first a...

Resolved! how to using sdram on touchgfx???

Hi guys, it's me.In the morning when i started my project i saw mcu's memory area looks like SDram is not working and i asked if FLASH is full will mcu have data to ASSETS FLASH? And why don't we exploit the two together to increase their size??  t...

_legacyfs_online_stmicro_images_0693W00000bje91QAA.png
OWLchan by Associate III
  • 2123 Views
  • 1 replies
  • 0 kudos

Saving data in QSPI Flash | STM32F469i-DISCO

Hello, I'm a total beginner and I'm looking to store some user data in the QSPI Flash,, but I don't really know how to proceed can you help me ?First, I changed the flash memory size in the .ld file from 16M to 12M so that TouchGFX won't overwrite m...

MFOWE by Associate II
  • 9146 Views
  • 15 replies
  • 0 kudos

STSAFE: Bring Up Tutorials

Hello,I am using a Nucleo-F401RE board with the X-Nucleo-SafeA1 expansion board (which claims it is compatible with any Nucleo development board). I am trying to use the software package that is shown in the link below:https://www.st.com/en/embedded-...

KMew by Senior III
  • 2467 Views
  • 2 replies
  • 0 kudos

Resolved! The custom made external loader, failed to make multiple Reads, (STM32CubeProgrammer returns error)

I follow the guide to make an external loader and it works for the most part. I can erase sectors, write data. But I can only read data once. If I try make multiple Read, STM32CubeProgrammer returns error. See example below:Example:14:56:32 : Time el...

_legacyfs_online_stmicro_images_0693W00000bjOrgQAE.png _legacyfs_online_stmicro_images_0693W00000bjOrlQAE.png _legacyfs_online_stmicro_images_0693W00000bjOtSQAU.png _legacyfs_online_stmicro_images_0693W00000bjOrbQAE.png
AJack.5 by Associate II
  • 7811 Views
  • 6 replies
  • 0 kudos