STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1740 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4888 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9586 Views
  • 5 replies
  • 3 kudos

Regular Conversion Manager Hang on EOC

I am essentially experiencing the exact same issue as this poster.  I have a single conversion registered, on ADC1 channel 13. It works great for ages, and then the RCM_execRegularConv function gets "stuck" waiting for end of conversion.   I am runni...

MCSDK debug error

Hi,Im currently tring to program my nucleo-f103rb module. I have succesfully generated Motor control workbench project and CubeMx project. After code generation using cubemx , stm32cubeide1.8.0 opens the project code. Without changing anyting on the ...

qqwq.1 by Associate II
  • 3549 Views
  • 7 replies
  • 0 kudos

Resolved! B-G473E-ZEST1S UM3118

Where to find user manual UM3118 referenced in B-G473E-ZEST1S Data Brief.The link to this manual in the data brief goes to Page Not Found.Many thanks.

elgeeds by Associate
  • 4353 Views
  • 2 replies
  • 0 kudos

Motor profiler - BLDC

I am trying to identify the motor parameters of a BLDC (with a multipolar magnet rotor) using Motor Profiler. Should I select SM-PMSM or I-PMSM in magnetic built-in?Thank you in advance for your answer. King regards,Cristhian Chavez Thank you in adva...

motor_prof.png

Resolved! Discontinuous PWM MCSDK

I have enabled the Discontinuous pwm and ran the motor but it started rotating in reverse direction compared to when none is enable. With no Discontinuous mode all features are validated, now i want to test all of them with Discontinuous mode enabled...

SRedd5_0-1697128464745.png
SRedd.5 by Senior III
  • 2069 Views
  • 2 replies
  • 1 kudos

Resolved! USB/com interface not working in STEVAL-SPIN3204/Windows10

Hi, I am new to ST evaluation board. I am trying to connect STEVAL-SPIN3204 board to a windows 10, and it is not working.In more details: The board is working with stsw-link007 (ST-LinkUpgrade) and loads the recent driver version (V2J43M28). The USB ...

ranrang by Associate II
  • 12224 Views
  • 12 replies
  • 0 kudos

NTC thermistor gain calculation for Board Manager

Can anyone explain to me how to calculate the "gain" property for a "NTCThermistor" hardware variant?The NTCs we use (NTCS0805E3103FMT) are not linear, so a "Thermistor gain in mV/°C" as mentioned in the wiki doesn't apply.As a side note: The wiki sa...

DMeie.2 by Senior II
  • 2735 Views
  • 4 replies
  • 1 kudos