STM32 MCUs Motor control

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Second NTC_Handle_t type sensor

uC = STSPIN32G4second sensor = PA4 (ADC2_IN17)I have tried add second NTC sensor and using MC functions.A have added:sConfig.Channel = ADC_CHANNEL_17; // BEARING_TEMPERATURE sConfig.Rank = ADC_REGULAR_RANK_1; sConfig.SamplingTime = ADC_SAMPLETIME_4...

ketchup by Associate III
  • 284 Views
  • 1 replies
  • 0 kudos

Resolved! How to configure 3 Shunt 3 ADC measurement

Hi,I have a STM32G491 based design with three differential shunts, routed to the three Op Amps of the MCU. I would prefer to run the Op Amps in standalone mode. This would allow me to have a low pass filter (cap across negative and output) and I woul...

JKolj.1 by Associate III
  • 803 Views
  • 3 replies
  • 2 kudos

ADC Interrupt Generation difference

I am bit confused with ADC interrupt code generated for my project compared with the code generated from the motor control SDK for the evaluation board B-G431-ESC1.For my generated code void ADC1_2_IRQHandler(void){ /* USER CODE BEGIN ADC1_2_IRQn 0 *...

SRedd.5 by Senior III
  • 264 Views
  • 0 replies
  • 0 kudos