Dear MCSDK users,
MCSDK version 6.3.2 is now available: Download It here.
This is a bug fix release and here are the main changes for this version:
Motor Control Features:
FOC
Fixed CORDIC Modulus computation in case of negative alpha value Fixed iss...
If, when generating a project, "attr not supported : Dmpu" Error message is reported, please ignore it for now. Issue is under investigation, and it does not prevent the project to be fully generated.
Dear MCSDK users,
MCSDK version 6.3 is now available: Download It here.
Here are the main changes for this version:
Motor Control Features:
FOCAdded C0 single shunt topology support.6StepThis algorithm has been enhanced on MCSDK version 6.3 release ...
Hello @socjcare,
Refer to User Manual documentation available through "Workbench tool">About>Documentations>Documentation>"User manual", "Open Loop Description and Usage" link.
Refer also on previous posts:Solved: Re: IHM17M1 For Motor profiler can't...
Hello @hyden_a_mist,
You are right for the documentation, thanks for the reporting. By default, in current use case, BKIN1 is used and connected to PA6, and BKIN2/DAC/TIM1_CHIN signals are not used.Could you share your project (at least .stwb6 and .i...
Hello @dfshea,
Bus voltage feature has to be defined on your board description and aligned with your hardware (EVSPIN32G4 example):
If TIMx_BRK_M1_IRQHandler() is called, you have to check why OCP occurred. Check if the Current Sensing Hardware Va...
Hello @socjcare,
If you are using MC SDK 6.3.2, refer to User Manual documentation available through "Workbench tool">About>Documentations>Documentation>"User manual" tab, "Motor Profiler Application Note" link:Progress execution bar stays at 28%The ...