STM32 MCUs Motor control

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MCSDK / FOC SDK for STM32F2

Hello, I have read that the support for STM32F2 in FOC SDK / MCSDK is skipped after 4.x. Is that right, if so, where can I get the latest 4.x version for my STM32F2 design? Thanks in advanced

MiJes by Associate
  • 331 Views
  • 1 replies
  • 0 kudos

pin level when disabling pwm

I'm using a general-purpose timer to generate low level pulses, configuring one channel as PWM. The problem is when I disable the channel, the signal goes low, and I want it to remain high.I played with the OCPolarity and PWM modes 1 and 2, but only ...

DAlvarez by Associate II
  • 651 Views
  • 4 replies
  • 0 kudos

debug the TMC5130 eval board

helloi am working with the TMC5130 eval kit. its a motor control driver that is controlled by STM32f205 chip.the IDE is based on eclipse IDE, and for now all i can do is build my project (there are few build configuration files) and program it via US...

Aasaf.1 by Associate
  • 333 Views
  • 1 replies
  • 0 kudos