STM32 MCUs Motor control

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error when generating code with MC Workbench 6.3.0

Hello there,I am currently working on a project considering the B G431B ESC1 and a BLDC motor.My goal is to control the motor through a external PWM Signal from a nucleo board.So far I could only control the BLDC motor through the MC Profiler and onl...

STMBatu by Associate II
  • 185 Views
  • 7 replies
  • 0 kudos

Motor speed issues B-G431B-ESC1

Hi!Trying to use a Leopard LC2830-980KV motor with the B-G431B-ESC1. I have managed to program the device with the MC Workbench and can run the motor using the Motor Pilot software. However I can't seem to get the speed over 2100 rpm for some reason....

Skärmklipp3.PNG Skärmklipp4.PNG Skärmklipp2.PNG

6-step OPEN-LOOP

Hello, MS_Workbench 6.3 created a project SM-PMSM motor  24V  Six-step control with OPEN-LOOP support. Successfully generated files, launched CubeMX. Then I generated a project for the Cube IDE. When trying to build the project, an error first appear...

MCSDK 6.3.0 is out!

Dear MCSDK users, MCSDK version 6.3 is now available: Download It here. Here are the main changes for this version: Motor Control Features: FOCAdded C0 single shunt topology support.6StepThis algorithm has been enhanced on MCSDK version 6.3 release ...

GMA by ST Employee
  • 193 Views
  • 1 replies
  • 2 kudos

Resolved! MC Workbench 6.3.0 - Generation of project fails.

Hello there,I am new to the MC Workbench and must configure the B-G431B-ESC1 to use it with a A2212/6T 2200KV Brushless DC Motor.I created a new project in the MC Workbench 6.3.0 and tried generating the project. Once the generation is completed I re...

STMBatu_0-1715772920498.png
STMBatu by Associate II
  • 2472 Views
  • 2 replies
  • 2 kudos

bus current

I would like to implement a feature,During motor operation,Increasing loads,By controlling the rotational speed,so that when the bus current reaches a given value, it does not increase any further,What should I do?

iskan by Associate III
  • 76 Views
  • 0 replies
  • 0 kudos

Speed mode and torque mode switching

Hi, I would like to realize switching between speed mode and torque mode during motor operation, but I found that there is a stuttering sensation in the motor when switching, how can I avoid this phenomenon?

iskan by Associate III
  • 98 Views
  • 0 replies
  • 0 kudos

How to control a Maxon BLDC with hall sensors

Hi,I'm trying to drive a Maxon 574741 BLDC motor with hall sensors, using your STEVAL-SPIN3204 evaluation board. I have installed MC Workbench, STM32CubeMX and the STM32CubeIDE. I'm rather new to motor control and the parameter setup for my motor in ...

LeiSve by Associate
  • 162 Views
  • 0 replies
  • 0 kudos