STM32 MCUs Motor control

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Wrong period values during motor startup.

I am making a BLDC motor controller using STM32G030C8t6. This microcontroller has a hall sensor sensing capability known as ‘Hall Sensor Mode / XOR Mode’. This generates an interrupt when any one of the three channels toggle. We are taking the timer ...

Untitled (2).png
Gladson by Associate III
  • 507 Views
  • 4 replies
  • 0 kudos

Resolved! MCSDK inverter

I'm using mcsdk and want to create an inverter file based on STM32G070CBTx, but when generating the project, it tells me that my selected hardware is not compatible with the algorithm

iskan by Associate III
  • 723 Views
  • 7 replies
  • 0 kudos

Resolved! How to run motor in Open Loop

HiI am running on a STM32G071 board, with my own custom HW (standard 3 phase halfbridge). The control is FOC sensorless with 1 shuntI am having problems tuning the motor, but for starters I would like to run the motor at low speed in open loopI can f...

KKrag.1 by Associate II
  • 1315 Views
  • 7 replies
  • 0 kudos