MCSDK 6.2.1 Firmware Fault Detection
I can't create a motor profile in MCSDK Workbench. I'm getting an error like the one below. What is the reason for this?
I can't create a motor profile in MCSDK Workbench. I'm getting an error like the one below. What is the reason for this?
I am making a BLDC motor controller using STM32G030C8t6. This microcontroller has a hall sensor sensing capability known as ‘Hall Sensor Mode / XOR Mode’. This generates an interrupt when any one of the three channels toggle. We are taking the timer ...
I'm working on a project whith use a STM32F407 MCU to control a bldc motor and also has a low power mode, the mcu will into stop mode.Now the stop mode is working, and we have issue to control the motor after wake up from stop mode.the code to enter...
STM32F405MCSDK = V5.4.5f_pwm = 10kHzHigh frequency task = 10kHzMedium frequency task = 1kHzPosition and speed = Hall (main) & STO+PLL (auxiliary)Current sensing = 3 x 3mOhm shuntsI am having a problem with very poor Id and Iq measurements when the mo...
Posted on November 30, 2017 at 12:57Greetings!For the past few weeks, I have been working with the SPIN3201 Eval-Board to control a small BLDC motor which is usually used for electrical-powered Longboards. I have chosen a purposely slow model with o...
Posted on October 12, 2017 at 12:36Hello,I'm facing an issue regarding low power on stm32l073. On my nucleo board NUCLEO-L073, when i go in stop mode, my consumption is around 1 and 3uA, so all seem to be ok. Then, we decided to make our own board (...