STM32 MCUs Motor control

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

may be a bug in the MC workbench

Hello, in the code I generated using MC workbench 5 or 6, there is something wrong with the part of the code that calculates the phase current value.You can easily find it by searching in the generated codePHandle->PhaseAOffset >>= 3;PHandle->PhaseBO...

Ywang.3 by Associate
  • 79 Views
  • 1 replies
  • 0 kudos

Acim Gui

Hello;I haven't found the ACIMGUI under the files or Motor workbench. Can i take old version or recently versions links?  

Resolved! Bug Report: Unimplemented Registers

Hardware: EVSPIN32G4-DUALConfiguration: 1-shunt FOC, Observer + PLL Bug location: register_interface.cRegisters in Question:FLUXWK_BUS_MEASMC_REG_PULSE_VALUE, MC_REG_BEMF_ZCRMC_REG_BEMF_UMC_REG_BEMF_VMC_REG_BEMF_WDescription:When these registers are ...

ccut93 by Associate III
  • 176 Views
  • 1 replies
  • 0 kudos

motorbench 6.2.1 with cube MX

Hello,I have intsalled the motorbench version 6.2.1, and I have already the cubeMX version 6.9, but when I'm using the motorbench and trying to open an example for the steval-spin3201, it's working until I reach the generate program and it's saying a...

Dandan0707_0-1713341768523.png

Resolved! Bug Report - ASPEP Protocol Ping Packets

Hello,I am currently trying to implement an ASPEC Controller in C# to communicate with a motor control dev board over the UART (essentially, creating motor pilot with the ability to modify as needed).  So far, I have implemented Beacon and ping packe...

ccut93 by Associate III
  • 725 Views
  • 3 replies
  • 0 kudos

Bug: RTOS task scheduler too fast

MCWB Version: 6.2.1CubeMX Version: 6.10.0Issue: I generate a default project for the B-G431-ESC1. Only settings I change is to enable the FreeRTOS with TIM6 as the tick timer. Firmware Package Version is V1.5.1 (Recommended).Via CubeMX I add a GPIO o...

DMeie.2 by Senior
  • 348 Views
  • 6 replies
  • 0 kudos