cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Motor Control SDK FreeRTOS

TimRocky
Associate

In STM32 MC SDK Workbench, is it necessary for me to tick the choice "Enable MC IRQ to use FreeRTOS Functions" when I enable FreeRTOS? In what circumstances should I tick this option? What happens when I don't enable this functionality? Anybody else knows? Screenshot 2023-09-19 144115.png

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Zied b.
ST Employee

Hello @TimRocky 

Ziedb_0-1695211967867.png

after investigation, as you can see on the left the .ioc with the option activated and on the right deactivated.
When you activate the options, the priority of certain interrupts is changed to allow the operation of the motor control part.

 

If you agree with my answer, please accept it by clicking on "Accept as solution".