With the new generated Code i receive a lot of errors like 0F 04 04 C0 0F 04 04 C0. TO control my SPIN3201 Board with the Motor Pilot works fine. By trying to send the same Data as the Gui (Voltage, Speed, Power....690100B0110019005900591B9900D105910...
Hi, I'm trying to control a BLDC motor via a B-G431B-ESC1 and an Arduino Mega. The Mega will be the master and send commands to the board. For ease of use, I'd like if it these were strings. I have found examples of how to use UART in an STM32 applic...
Hello @allThe following problem hunts me since some weeks: I use a custom motor control PCB based on STM32G431CBU. Communication via UART works great through motor pilot but as soon as I start the motor, the comunication is gone and I cant stop the m...
I am trying to transmit repeatedly using HAL_UART_Transmit_DMA(). The first transmit works. All following fail. The HAL_UART_TxCpltCallback() does not fire. All information I can find on this says you have to check the box 'USART1 global interrupt/.....
I am using the motor control code in the cube IDE generated by the motor workbench . How can I send back the speed of the motor to the console? Can I use HAL_Uart? Right now I am not getting any response
Hi ST,I am unable to establish UART communication between ST MotorPilot and STEVAL-SPIN3202.I am uploading one of the two STEVAL-SPIN3202 examples.Setting up 9600 baud rate (same as in Cube MX settings). Using correct COM port.Hardware setup: Power ...
I have a motor control board built around the STM32F446RET6. I was updating code using motor control workbench to alter the control parameters.After an update, I was no longer able to use the motor control workbench console to communicate with the bo...
(Environment)MC_SDK 5.Y.3 + STM32CubeMX 6.3.0 with HAL + IAR EWARM 8.5(Hardware)custom board based on F446RE + custom power board + Low Voltage BLDC motor with Encoder(What I found)I configured UART5 to the serial communication.In "mcp_config.h", US...
I'm trying to use this board to develop the serial I/O "user interface" for my application but I don't have my custom board yet.