User Activity

Hi. I've got a sensored 14-pole motor that does 3000rpm max, but I can't get it to go past 300rpm in the MotorControl Pilot.I've confirmed its phase resistance and inductance with the ST Profiler, the VESC Tool Profiler, and the manufacturer.I've con...
I thought my hall sensors were originally broken because I didn't see them giving a 5V signal. After replacing them, I see that new ones give at most 0.25V when in the presence of even a strong magnet! Turns out some hall sensors come with an integra...
Hi, I have a 14-pole outrunner that's rated for 30A, but I get an overcurrent error every time. That changed when I tried changing its max current from 30A to 5A. I still get two problems: 1) the motor never snaps to set speed, only oscillates about ...
Electronic Speed Control Debugging? What does this setting do?
Hi, I'm getting some nonsense values in Motor Pilot under "MC Configuration". It says there is no max app current or voltage, and my PWM frequency is something ridiculous. I've tried changing it to 25kHz and 20kHz, and these were the readings. I've n...
Kudos from