MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! why IIS3DWB timestamp values are zero ?

I have timestamp counter enabled and batching to FIFO with decimation=1. I can see the timestamp values are interleaved with the accelerometer values, but the timestamp values are always 0 like this (this is SPI trace):22 00 00 00 00 00 0A12 32 F7 2F...

mete by Senior II
  • 1446 Views
  • 4 replies
  • 0 kudos

Resolved! LIS3DH Single/Double Tap Detection Current Consumption

Hi,We notice that LIS3DH accelerometer has multiple mode which can be utilized to be used on low power mode for single/double tap detection. Does single/double tap detection increase the current consumption stated on the data sheet/design tip?https:/...

Dillah by Associate II
  • 3060 Views
  • 11 replies
  • 0 kudos

Resolved! LSM303AGR gives weird values output of the accelerometer

Hi,I am using examples from the github repo to test accelerometer. I can read device id from both accel and magnetometer. Also I can read back the registers I set.  However, when it comes to read accelerometer, I read same values from all axis of the...

Resolved! LIS2DE12 mangles REG1 register

I'm attempting to use the LIS2DE12 in perhaps the simplest configuration: To directly poll the X,Y,Z registers as needed. I'm using the I2C bus. At this point, I've added some debug checks, so the current process looks like this: 1. On wakeup, I read...

Resolved! LIS2MDL magnetometer

Hi Team,We are using the LIS2MDL magnetometer sensor in the I2C connection on the xilinx zcu106 evaluation board, which we are connecting to i2c0.We are using the default Linux driver for lis2mdl.https://github.com/Xilinx/linux-xlnx/tree/xlnx_rebase_...

Ranjithkumar_0-1707455603356.png Ranjithkumar_1-1707455971604.png

Question about STEVAL-STWINKT1B

SpoilerHello everyone,I received a STEVAL-STWINKT1B to conduct research about predictive maintenance, and right now I need to get some data into my computer through USB. I have installed FP-SNS-DATALOG1 on it. I followed the manual for the particular...

ed4b0757-7b59-4f67-8f78-1b7914f32481.png NomadRTU_0-1707572571508.png
NomadRTU by Associate
  • 716 Views
  • 0 replies
  • 0 kudos

Resolved! STHS34PF80 threshold set

Hello community,my sths34pf80 is connected with a wireless MCU through I2C in fast mode. during the initial process the function " sths34pf80_presence_threshold_set(&presenceHandle, 200); " is called, sometimes there is no problem, the sths34pf80 can...

Danny0007_0-1706307943338.png Danny0007_1-1706308318480.png