MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSV32X ODR Accuracy

Good Afternoon,I've been working on migrating from the LSM6DSO32 to the LSM6DSV32X and I notice that neither part specifies ODR Accuracy for normal or low power modes.  Is this information available? Thank you

Looking for Accelerometer

Hi, I am looking for an accelerometer. I wonder if there is any ST MEMS chip that meets my requirements:I don't need very high max G force: 4/8G should be enoughLow power consumptionAble to send trigger, like a GPIO rising or falling signal, when acc...

HDaji.1 by Senior
  • 1030 Views
  • 1 replies
  • 0 kudos

LSM6DSL big gyroscope fluctuations on acceleration

Hello, I am using a LSM6DSL sensor and when applying a 2G acceleration without rotating the board, I get very important spikes on the gyroscopes of about -90°/s to +90°/s amplitude.This is very strange. Is this a normal behaviour from this sensor ? A...

lsm9ds1-gyroscope

Hi,I have an application with LSM9DS1 sensor and I expected that when I change LSM9DS1 sensor position from horizontal to vertical value will change but changed only when sensor was moving but after that valus comes almost same for horizontal or vert...

JarekG by Associate
  • 1352 Views
  • 1 replies
  • 0 kudos

Resolved! IMU Sensor Fusion Performance

Hi Team,I searched sensor fusion performance information of LSM9DS1TR, LSM6DSO IMUs as below,1. Static Accuracy (Yaw, Pitch, Roll) = ?2. Dynamic Accuracy (Yaw, Pitch, Roll) = ?3. Orientation Settling time = sec?However, I did not find it in the respe...

VB.4 by Associate II
  • 1314 Views
  • 1 replies
  • 0 kudos

MEMS Studio Path: resample_odr.exe does not exist.

In MEMS Studio under advanced features > MLC I upload a data pattern and label it under the "Data Pattern" tab. On the "Datalog analysis" tab when I click the Run button it gives the following error.Path: resample_odr.exe does not exist. Please check...

LosKlong_0-1724496672445.png LosKlong_1-1724496895495.png
LosKlong by Associate
  • 1394 Views
  • 1 replies
  • 0 kudos

Resolved! Sensortile in cradle is not working with microsd card

Hello all, I wanted to use sensortile to collect data on microsd card. (I have two of them) So, One portable cradle from the kit working good, but another is not working with the same microsd card. When start it from the android app the sensor just b...

Boris- by Associate
  • 1805 Views
  • 2 replies
  • 0 kudos