MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ILPS28QSW Gel Info

Hello all,I am looking for more info on the gel used with ILPS28QSW.We want to use it in an application where the sensor may be submerged in 10% to 40% alcohol v/v for extended periods of time. Will the sensor be okay? Or is there another product whi...

Resolved! IIS3DHHC Sensitivity

Regarding the sensitivity of IIS3DHHC, the datasheet says 0.076mg/digit. It is written. To be exact 5g/2^16 (= 0.07629mg/digit) Is that correct?Thanks!

totaw.1 by Associate II
  • 1570 Views
  • 2 replies
  • 0 kudos

STHS34PF80 Sensor's Power Consumption is very high.

Hello there, I am currently working on a project where I am prototyping STM32WL55 with an STHS34PF80 sensor to detect the presence. The presence detection is excellent and robust so far. However, the power consumption seems to be very high at the mom...

Can‘t pair with BLE Sensor Tile.Box Pro

I am not able to pair Sensor Tile.Box Pro with my iphone 13 over Bluetooth with the app ST BLE Sensor. When connecting I get prompted to enter number shown on the device, but the Tile.Box does not have a display, so that’s impossible. 

michal6 by Associate
  • 896 Views
  • 0 replies
  • 0 kudos

6-positions calibration

Hello,     I am developing on a custom boards with a STM32F407, LSM6dsv16x and LIS2MDL.On CubeMX I set the MotionFX package. Even selecting the MotionAC it looks like the library is not added to the output (is it correct?). The motionTL can be added....

MRaff.1 by Associate III
  • 1121 Views
  • 0 replies
  • 0 kudos