MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

INemo and LabView

Posted on July 09, 2013 at 07:17Hello, I'm very green when it comes to sensors and MCU. I'm tasked with implementing the INEMO v2 board to work with LabView independent of the INEMO GUI. Is this possible? How difficult will it be? Where should I sta...

Configuring FIFO mode in LIS3DH

Posted on June 24, 2013 at 19:58Hi,   I am trying to configure LIS3DH in FIFO/Stream mode and have a few questions as the data sheet is not very clear.1) Can I configure the INT2 as the WaterMark interrupt?  I don't see any option to configure INT2 ...

ramperry by Associate
  • 1093 Views
  • 1 replies
  • 0 kudos

offset error in LSM303D

Posted on June 24, 2013 at 18:40I have a design with the LSM303D e-Compass and 3D accelerometer.  When we calibrate the accelerometer, we are frequently seeing zero-g level offset corrections greater than the +/-60 milli-g typical value specified in...

LIS302DL problem

Posted on June 09, 2013 at 13:01Hi,I've been using an STM32F4 Discovery board with uVision4 for around 10 months now, and have learnt how to use the basic features (ADC, LCD, USART etc) and I'm now tackling the accelerometer (LIS302DL). I've looked ...

unable to use SPI interface

Posted on June 07, 2013 at 08:41I am trying to access the LSM330DLC devie using the SPI interface without luck. I have religiously tried to follow instructions in the part data sheet to read the WHO_AMI_G register but the there is no output on the S...

bnp979 by Associate III
  • 699 Views
  • 0 replies
  • 0 kudos

pdm filter

Posted on June 04, 2013 at 10:14libPDMFilter_IAR.a Does LibPDMFilter_IAR.a in the STMF4 DISCORVERY  is used for all STM32 family? for example, Is LibPDMFilter_IAR.a used for STM32F1XX not STM32F4XX????

sojaewoo by Associate II
  • 957 Views
  • 0 replies
  • 0 kudos

LSM303DLHC stuck on -4096

Posted on May 07, 2013 at 18:05We have two LSM303DLHC on one board. Sometimes one of them appears to be stuck at -4096 on some axes. Even when I wave a magnet close to it doesn't change. The next day it's ok. The board was sitting on my desk all day...

dimitar by Associate II
  • 832 Views
  • 0 replies
  • 0 kudos

Please help using LSM330D

Posted on May 03, 2013 at 06:25I am trying to get a gyroscope raw data using I2C. DEN_G is connected to MCU's GPIO and I set the register to use level trigger mode. I think I2C slave address is correct because when I read WHO_AM_I_G register I get 2...

suriko by Associate
  • 943 Views
  • 1 replies
  • 0 kudos

LSM303DLHC DRDY interrupt difficulties

Posted on April 23, 2013 at 19:05Greetings,I'm trying to bring up an LSM303DLHC and I'm having trouble getting any form of interrupt out of the device.I've taken an STEVAL-MKI119v1 and removed the MKI108v2 and jumpered it to my I2C bus.  I have Vdd ...

ste2e by Associate
  • 750 Views
  • 0 replies
  • 0 kudos