User Activity

I need stm32h​7 eval board usb host bulk in/out example programIs there any information? or example code?
Posted on January 03, 2014 at 03:11I evaluated L6470 & L6472 with unipolar not bipolar together. problem is that motor is not reached about 1500pps. It is stopped with very strong vibration about 1500pps. because of motor dc24v, I think that current...
Posted on December 16, 2013 at 09:50I use ST L6470 with unipolar motor. L6470 is biplar type dirver, so I unconnected com line of unipolar motor. motor spec is below:  MAKER: sanyo denki  type : 103H5210-0480  1.2A/1.8DEGREE/3.3OHM. because unconnec...
Posted on June 04, 2013 at 11:33 pdm filter libPDMFilter_IAR.a Does LibPDMFilter_IAR.a in the STMF4 DISCORVERY  is used for all STM32 family? for example, Is LibPDMFilter_IAR.a used for STM32F1XX not STM32F4XX????
Posted on June 04, 2013 at 10:14libPDMFilter_IAR.a Does LibPDMFilter_IAR.a in the STMF4 DISCORVERY  is used for all STM32 family? for example, Is LibPDMFilter_IAR.a used for STM32F1XX not STM32F4XX????