MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lis3lv02dq's ODR can not greater than 160Hz

Posted on October 10, 2013 at 02:52The RDY is used to indicate a new data is available. The problem is that the ODR can not greater than 160Hz,otherwise after a period of time of dataoutput,the RDY goes low,and the value of STATUS_REG is changed to ...

kdl6618 by Associate
  • 993 Views
  • 1 replies
  • 0 kudos

LSM9DS0 4-wire SPI communication

Posted on October 12, 2013 at 08:30hi,guysI'm working on LSM9DS0 with STMEVAL-MKI109V2,using 4-wire SPI communication?read gyro's WAI reg is ok if keep CS_G=0 and CS_XM = 1 after EVAL board power on, but if CS_G=0 after CS_G=1 and CS_XM = 1,read WAI...

poa by Associate
  • 1271 Views
  • 2 replies
  • 0 kudos

Dual LIS3DH Dilemma

Posted on November 05, 2013 at 10:01Hi, So time to get right to it, I am using 2 LIS3DH Accelerometers ( Two Different Addresses Assigned to them), they are both using the same I2C lines and the same INT line on my microcontroller. That is the way...

H3LIS332DL Interrupt events

Posted on October 23, 2013 at 11:48As Interrupt sources, what means the ''X/Y/Z High Event'' or ''... LOW Event'' in the datasheet? Are there defined trigger values for these events, and are they changeable in some registers? #h3lis331dl #acceler...

hmai by Associate
  • 1111 Views
  • 1 replies
  • 0 kudos

Finding land pattern for LIS3DH

Posted on October 22, 2013 at 16:32Hi,Where are the land patterns for LIS3DH, LLGA16 (3x3x1.0) 7983231 filed?I have tried searching for all of the above keywords but still come up empty handed, the closest i get is a land pattern by maxim, 90-0396.T...

interrupt generation problem during CTRL_REG3 setting in AIS328DQ

Posted on November 14, 2013 at 08:34Hi, The accelerometer was generating the interrupt when the value of CTRL REG 3 was  set to 0x80. But AS CHANGED TO 0x84 to check the latch interrupt request there is no more interruppt generation. Can anyone prov...

rehanar by Associate
  • 1026 Views
  • 1 replies
  • 0 kudos

L3GD20 data stability?

Posted on November 05, 2013 at 18:21Okay - I've got data flowing from the L3GD20 into the microcontroller using the DRDY/INT2 signal.  As I examine the readings that I am receiving from the sensor chip, though, it appears that I receive ''bogus'' va...

rich by Associate II
  • 1247 Views
  • 1 replies
  • 0 kudos