cancel
Showing results for 
Search instead for 
Did you mean: 

lis3lv02dq's ODR can not greater than 160Hz

kdl6618
Associate
Posted on October 10, 2013 at 02:52

The RDY is used to indicate a new data is available. The problem is that the ODR can not greater than 160Hz,otherwise after a period of time of dataoutput,the RDY goes low,and the value of STATUS_REG is changed to 0x77(why??). The initial code follows:

Write_Command(CTRL_REG1, 0xE7);

Delay_Time(10);

Write_Command(CTRL_REG2, 0x14);

Delay_Time(10);

Write_Command(CTRL_REG1, 0xE7);

Write_Command(CTRL_REG3, 0x18);

Delay_Time(10);

Write_Command(CTRL_REG2, 0x44);

Delay_Time(10);

#lis3lv02dq
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Thiago REIS
Associate II
Posted on November 18, 2013 at 17:00

Hello Kong,

In order to better answer your question, could you please send me the registers setup of your sensor?

In special

CTRL_REG2 (21h).

Thank you very much,

Thiago Reis