MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Urgent:Data Ready Interrupt

Posted on December 06, 2013 at 12:00Hi, I don't know, the interrupts work. I have the testcase attached. Here is the logged sequence: BEGIN: STAT_REG = 0 .. STAT_REG = 0xF // here should come the Int, shouldn't it? .. STAT_REG = 0xFF // Overflow, ne...

steffen by Associate II
  • 1996 Views
  • 3 replies
  • 0 kudos

LSM9DS0 12 gauss and 8 gauss range of the magnetometer

Posted on November 06, 2013 at 17:41Good morning, I am having some trouble in working with the magnetometer with the 12 and 8 gauss range. I am using an SPI communication. All the data from accellerometer and gyroscope are correctly  as well as fo...

marco23 by Associate II
  • 1402 Views
  • 3 replies
  • 0 kudos

LSM9DS0 Reference design and code

Posted on December 19, 2013 at 20:05Can anybody point me to any additional reference material on the LSM9DS0.  Such as any reference designs and source code.  Interested in proper implementation of read/write sequencing.  Thanks. #lsm9ds0-referen...

jeffd by Associate
  • 626 Views
  • 0 replies
  • 0 kudos

startup for the LIS331DLH accelerometer

Posted on November 28, 2013 at 07:09hi guys, i am working with the LIS331DLH accelerometer, i was able to read the product ID but when i am going to set the config register 1  i am not getting acknowledgement, what may be the cause? #lis331dlh

data format

Posted on November 30, 2013 at 16:19 I've just read the thread: Data output format of the LSM303DLHC the accelerometer data is left�?justified, in normal mode, the data is in 12�?bit representation which means the lowest 4 bit in LSB are always 0s I...

steffen by Associate II
  • 1396 Views
  • 3 replies
  • 0 kudos

LSM303DLHC as outdoor thermometer

Posted on December 11, 2013 at 08:06I want to use lsm303dlhc as outdoor thermometer. I use next code       int8_t value= 25+data[0];        uint8_t sign=value&0x80;        uint8_t cels=0;        if(sign)            cels=(~value)+1;        else     ...

DRIVER EXAMPLE FOR LSM330DLC

Posted on December 09, 2013 at 13:31Hello to all, In order to ease the self learning process and setup ST's LSM330DLC, attached to this post is an example of its drivers setup for a general application. Thank you, Thiago Reis #lsm330dlc

Drivers Examples for LSM303D

Posted on December 09, 2013 at 13:29Hello to all, In order to ease the self learning process and setup ST's LSM303D, attached to this post is an example of its drivers setup for a general application. Thank you, Thiago Reis #lsm303d

Driver Example for L3GD20

Posted on December 09, 2013 at 13:20Hello to all, In order to ease the self learning process and setup ST's L3GD20, attached to this post is an example of its drivers setup for a general application. Thank you, Thiago Reis