Posted on April 25, 2013 at 16:47I have the stm32f4 discovery board usb connected. Debugging works but the command printf doesn't work (trace: no synchronization).System clock is set 168Mhz, SWO 2MHz. Any idea?Thank you
Posted on November 05, 2012 at 11:58I have the STEVAL-MKI062V2. I erased the original flash contents and downloaded my own code.Now I want to put again the old flash content to use with the iNEMO Suite application. I have the iNEMOV2_Firmware_Packag...
Posted on August 07, 2012 at 14:38I work with the gyroscope LPR430AL. The pitch angle works fine, the roll angle results in some strange values... (if I turn the module of 90° in roll angle I measure the right value of 90°. When I come back to 0°...
Posted on August 07, 2012 at 09:38Hello,I implemented the RTC example of ST (calendar, time counter) but it seems to work just with an interval of 1 second. I need it to work with an interval of 1ms. How can I do it?Thank you!Best regards