MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to interface 4-wired SPI with interface LSM9DS0?

Posted on October 10, 2013 at 08:29I'm designing with LSM9DS0. And my goal is interface a 4-wired SPI with the MEMs device. This is my interface design. I add a 3:1 mux for interface 2 SDO pins into a MISO. I want to know that my approach is suitabl...

0690X00000604wmQAA.png
just4u78 by Associate II
  • 1681 Views
  • 4 replies
  • 0 kudos

Data Ready Interrupt in LIS2DH

Posted on February 24, 2014 at 15:03How to configure LIS2DH in interrupt mode for Data Ready(DRDY1). I am stuck on this one.I have tried both latched and pulsed interrupts.I have configured INT1 pin for Data ready Interrupt.But it is not working. Pl...

LSM303D Noise levels?

Posted on June 10, 2014 at 12:58I am using an LSM303D and find the noise level surprisingly high. I have configured it with the following parameters:#define CTRL0 0b00000000 //for normal mode, filters by-passed#define CTRL1 0b00011111 //update afte...

feverest by Associate
  • 1052 Views
  • 1 replies
  • 0 kudos

Inemo-M1 'LSM303DLHC_AccDataReady.c' problem

Posted on June 18, 2014 at 14:24Hi guys,I have jsut started using the Inemo_m1 discovery board.After Installing the software and doing some hello world projects (using KEIL IDE;debugged via ST-Link debugger), I decided to setup communication with th...

bouvett by Associate
  • 690 Views
  • 0 replies
  • 0 kudos

Problems with new iNemo Modules

Posted on June 17, 2014 at 17:25The old code I developed for other iNemo units does not work with parts just received.  It gets stuck at boot time.Code was based on suite INEMO-ENG-M1LI3_V5-1. It works ok when in debug via ST-link, but if left fee r...

franz by Associate
  • 679 Views
  • 0 replies
  • 0 kudos

About LSM330DLC Gyroscopes reflow solder problem

Posted on June 11, 2014 at 07:32We used LSM330DLC Gyroscopes in electric self-balancing unicycle. There is one problem of LSM330DLC  afterreflow solder. The LSM330DLC has offset to detect the angle from the vertical direction. The offset may be 0-7 ...

cac2012 by Associate
  • 755 Views
  • 1 replies
  • 0 kudos

MEMS Microphone Product Longevity

Posted on June 11, 2014 at 19:10Does ST have an expect product longevity for the MEMS Microphones?  These products look to be targeted at Consumer Products and there would be a concern of using these in an industrial product that needs a life expect...

gpowanda by Associate
  • 946 Views
  • 2 replies
  • 0 kudos

Code to Calculate Roll/Pitch/Yaw

Posted on June 12, 2014 at 18:00Does anyone know where to find/have the actual source code that calculates Roll/Pitch/Yaw for the iNEMO M1 System?I have the MKI121V1. Looking to see if it's possible to reset those values for calibration purposes, or...

mrm63 by Associate
  • 985 Views
  • 0 replies
  • 0 kudos

Extended Kalman Filiter

Posted on June 09, 2014 at 21:04Is the extended Kalman Filtering that's talked about in the iNEMO Engine LI3 (Lite) something that's already applied in the regular iNEMO suite when calculating Roll/Pitch/Yaw and Quaternion data? If I'm using the sof...

mrm63 by Associate
  • 946 Views
  • 0 replies
  • 0 kudos