Posted on July 21, 2014 at 18:30I wanted too know if it is possible to use the pro version of the engine on the M1 module, is the hw compatible?Thanks for the help
Posted on June 17, 2014 at 17:25The old code I developed for other iNemo units does not work with parts just received. It gets stuck at boot time.Code was based on suite INEMO-ENG-M1LI3_V5-1. It works ok when in debug via ST-link, but if left fee r...
Posted on January 29, 2014 at 18:47Hi,after installing and compiling the iNemo Libraries, I wanted to know if there are any code samples relating the M1 module, even simple ones.Thank you #inemo-m1-sample-code