User Activity

My goal is to connect 2 internal PGAs to 1 ADC (especially ADC2). I configured in CubeMX and generated source code.   However, when I checked the ADC channel initialization code in IDE project, I could see that only one channel is activated in ADC2....
I created a project using EVSPIN32G4-DUAL to test the two motor drive combination provided by ST. Then, the following error message was output. Generate ProjectWarning! Hardware changes must be applied to the following signals. Please, refer to the b...
I want to create a project with the Motor Control library using CubeMX. However, The Motor Control library is not registered as a software package in CubeMX, Now. Refering some application note, it says to use CubeMX's X-CUBE-MCSDK, but this software...
I am newbie of mc workbench.I'm in trouble with making custom board configuration of MC workbench. I think there are some restrictions for usage of MC workbench.When configuring 2 bldc motor settings, I want to receive individual PWM inputs, but I ca...
Posted on May 26, 2015 at 07:11I would like to use the PWM as clock source for other device. so I want to know the maximum frequency of PWM. As faster the frequency of PWM signal increase, the more the shape of PWM signal become to triangle signal. ...