MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3MDL offset

Posted on July 09, 2014 at 15:47I received some results from LIS3MDL.I tried to measure the magnetic field of the Earth = 0.05 mT = 0.5gauss. Full scale setting = �4gauss. If I rotate the magnetometer Y axis towards the north I receive 0xF3E0 (-3104...

glory_man by Associate II
  • 1180 Views
  • 1 replies
  • 0 kudos

LPY410AL Drive Strength

Posted on August 28, 2014 at 19:21I have a question pertaining to the drive strength of the analog outputs of the LPY410AL 2-axis analog gyroscope. The circuit is as follows: The analog outputs of the LPY410AL are connected to the inputs of a LMV324...

LIS331dlh I2C read problem

Posted on August 21, 2014 at 14:11Hi!I am using the LIS331DLH sensor in my project. I have no problem with processing between CPU and sensor via SPI. But I cannot communicate them via I2C - all registers are return 00 when reading.Here is the part o...

Using LIS331EB

Posted on August 12, 2014 at 12:51Where can  I find  all additional files for IAR (startup_lis331eb.s, StdPeriph_Driver, StdPeriph_Examples )? Should I use core_cm0.h or you can give me something like lis331eb.h? Thanks for the help. #lis331eb

ridelar by Associate
  • 797 Views
  • 0 replies
  • 0 kudos

LSM303DLHC reading 0x00 when enable both acc & mag

Posted on August 11, 2014 at 19:30 Hello, recently i started working on a project using LSM303DLHC, i noticed if i enable both accelerometer and magnetometer, i get 0x00 data. If i enable only the accelerometer, the data is normal on all three axis ...

Bogdan by Senior
  • 739 Views
  • 0 replies
  • 0 kudos

Noise cancellation algorithm code.

Posted on July 27, 2014 at 17:40Hi All,My name is Gil and our company is working on a wearable electronic system.As part of our system we intend to integrate an ST digital microphone P/N: MP34DB01TR.We want to use 2 microphones in order to implement...

gil by Associate
  • 628 Views
  • 0 replies
  • 0 kudos

how to tell if the LSM330 chip is dead

Posted on June 08, 2013 at 00:27My LSM330 chip is not responding to SPI communication. Is there a way to electrically tell if the chip is dead? Thanks.

bnp979 by Associate III
  • 1053 Views
  • 1 replies
  • 0 kudos