MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

iNEMO-M1 as SPI Slave

Posted on November 03, 2014 at 15:44Hello EveryoneI am working with the STEVAL-MKI121V1 board and Discovery-M1-Fw package, trying to get rid of the USB interface and replace it with SPI configured as Slave. My intention  for the the final system is ...

rasko by Associate
  • 913 Views
  • 1 replies
  • 0 kudos

PCB design guidelines

Posted on November 03, 2014 at 23:45Hello, I'm developing a compass module based on the LSM303D with a STM32F030x as host controller. I'm a little bit confused about the inconsistent PCB guidelines and application hints. In the application hints se...

marten by Associate II
  • 1032 Views
  • 0 replies
  • 0 kudos

LSM330D Self Test

Posted on October 21, 2014 at 16:28According to it's datasheet the LSM330D has a self test mode enabled by setting the self-test bit to 1 however there is no register entry I can find dor the self-test bit.Where is it ?

rhunt by Associate
  • 964 Views
  • 1 replies
  • 0 kudos

LSM330DL - DataRready Interrupt

Posted on November 20, 2013 at 10:38Hi community, i am working on an application with the accelerometer and gyroscope in LSM330DL. At the moment I try to use the DataReady-Interrupt for the gyroscope. My understanding of DRDY-Interrupt is that when...

pz by Associate II
  • 2882 Views
  • 6 replies
  • 0 kudos

LSM303D anti-alias filter

Posted on October 31, 2014 at 21:54I'm a bit lost about the use of the acceleration filter bandwidth. How to choose the relevant value between 50 and 773Hz ? -- Fabien #filter #lsm303d #accelerometer

how get INEMO software demonstration?

Posted on October 22, 2014 at 11:41how get INEMO software demonstration, the server seem out of order, I try 6 times I receive, illegal character and after the server is out of order, try later

yves2399 by Associate II
  • 752 Views
  • 0 replies
  • 0 kudos

iNEMO Engine M1 LI3 - ported to STM32F4 not showing coorect data

Posted on October 22, 2014 at 08:18Hello, i am using the iNEMO Lite soft version, namely INEMOEngineM1LI3,  the only thing i modified to work with the stm32f407 was some i2c functions, and the data/trafic on the i2c buss is ok. I tryied to display t...

Bogdan by Senior
  • 872 Views
  • 0 replies
  • 0 kudos

LIS3DSH SPI + resolution

Posted on October 21, 2014 at 10:33Hi, I have one question about the SPI of the LIS3DSH sensor. Does it have a multiple byte read bit? On page 26/53 (datasheet) in figure7 there is a MS bit, but in the text it is not mentioned. Where is the mistak...

truland by Associate
  • 913 Views
  • 0 replies
  • 0 kudos