MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Tap detection

Posted on September 08, 2011 at 16:49Hi,    I am trying to do double tap detection at 10hz and 25hz .Is this possible at low frequency. Viewing the acceleration graphs in Inemo PC suite I could see that the response is poor at low frequency and good...

1.8v Digital Power supply for accelerometer

Posted on April 09, 2011 at 20:49Hi,   Could someone tell me what is the reason for having a 1.8V supply for the digital I/O of the accelerometer.One reason Im guessing could be lower power consumption and compatibility with lower voltage peripheral...

Inemo Dfuse problem

Posted on August 12, 2011 at 10:23Hi,    I am currently developing a PC application for STM32 using Inemo board.The PC application will be able to upgrade the firmware of the STM32 using Dfu mode. Iam using Visual studio Vb.net for the PC side appli...

How can I write to the SD card

Posted on August 08, 2011 at 23:47Hi all.Sorry for the simple question, but I'm totally new to this but how can I write the sensor output to the SD card? I can't seem to find info on it in the documentation.My intention for using the board is for Da...

gummih by Associate
  • 843 Views
  • 1 replies
  • 0 kudos

iNEMO V2 alignment with 3D cube for perfect rotation

Posted on August 04, 2011 at 09:27HiCould anyone tell  how to align iNEMO V2 Board with 3D Cube (on monitor) to see the perfect rotation. ST provides a small 3D Cube demo, it's ok. I want to the in my VC++ program to accomplish the same alignment.1....

harinath by Associate III
  • 558 Views
  • 0 replies
  • 0 kudos

Download software on the board without debugging

Posted on July 28, 2011 at 12:35Hello, After downloading my software on the board, it only can executes when I am in debugging mode and make a RUN. When I restart the board without debug, my software isn't effective anymore, whereas it's supposed t...

Inemo Source for Commercial products

Posted on July 09, 2011 at 10:44Hi,We have purchased the Inemo V2 board and are happy with all the functionalities it has to offer. The reason for buying the board was to evaluate ST's platform before using ST MEM's components in a commercial produc...

royston by Associate II
  • 621 Views
  • 2 replies
  • 0 kudos

How to get Accelerometer(LIS303DLH) data in ''g'' units ?

Posted on July 18, 2011 at 05:16HiCan someone tell me how to get accelerometer data in ''g'' units.The data we get form iNEMO V2 is ''short int'' now which is output of ADC.In iNEMO Suit GUI, we can see the data in ''g'' units.How to get this, I mea...

harinath by Associate III
  • 437 Views
  • 1 replies
  • 0 kudos

installing the iNemo2 firmware

Posted on February 26, 2011 at 04:53 Hi Folks, I bought the iNEMO V2 evaluation board. It has the demostration firmware on it. I would like to use this board as a complete system since it has all the sensors on it. So, will I be able to inst...

kirank by Associate II
  • 1491 Views
  • 8 replies
  • 0 kudos