MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS331dlh I2C read problem

Posted on August 21, 2014 at 14:11Hi!I am using the LIS331DLH sensor in my project. I have no problem with processing between CPU and sensor via SPI. But I cannot communicate them via I2C - all registers are return 00 when reading.Here is the part o...

Using LIS331EB

Posted on August 12, 2014 at 12:51Where can  I find  all additional files for IAR (startup_lis331eb.s, StdPeriph_Driver, StdPeriph_Examples )? Should I use core_cm0.h or you can give me something like lis331eb.h? Thanks for the help. #lis331eb

ridelar by Associate
  • 570 Views
  • 0 replies
  • 0 kudos

LSM303DLHC reading 0x00 when enable both acc & mag

Posted on August 11, 2014 at 19:30 Hello, recently i started working on a project using LSM303DLHC, i noticed if i enable both accelerometer and magnetometer, i get 0x00 data. If i enable only the accelerometer, the data is normal on all three axis ...

Bogdan by Senior
  • 545 Views
  • 0 replies
  • 0 kudos

Noise cancellation algorithm code.

Posted on July 27, 2014 at 17:40Hi All,My name is Gil and our company is working on a wearable electronic system.As part of our system we intend to integrate an ST digital microphone P/N: MP34DB01TR.We want to use 2 microphones in order to implement...

gil by Associate
  • 458 Views
  • 0 replies
  • 0 kudos

how to tell if the LSM330 chip is dead

Posted on June 08, 2013 at 00:27My LSM330 chip is not responding to SPI communication. Is there a way to electrically tell if the chip is dead? Thanks.

bnp979 by Associate III
  • 579 Views
  • 1 replies
  • 0 kudos

About LPS331AP

Posted on January 10, 2014 at 07:53I am sorry that I post a question about pressure sensor at accelerometer forum, but I can't find a forum about barometric pressure sensor. I hope to know the wake up time of the chip from the power down to ready st...

hitwch by Associate II
  • 1976 Views
  • 6 replies
  • 0 kudos

Solution versus ADXL203

Posted on July 23, 2014 at 16:56I am looking for the best option versus this ADI part. Key requirements are - powered by 3.6V DC.- zero g temperature stability of 0.1 mg/C or better.- resolve angles down to 0.5 degrees at least, 0.1 degrees preferre...

PI3P on M1 module??

Posted on July 21, 2014 at 18:30I wanted too know if it is possible to use the pro version of the engine on the M1 module, is the hw compatible?Thanks for the help

franz by Associate
  • 482 Views
  • 0 replies
  • 0 kudos

H3LIS331DL 3-wire SPI

Posted on July 20, 2014 at 11:01H3LIS331DL accelerometer has 3-wire SPI mode. What i will get in this (3-wire) mode at pin number 7 (SDO in 4-wire mode). Is it pull down, pull up or open drain ?

tomasz by Associate
  • 664 Views
  • 0 replies
  • 0 kudos