MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DSH INT1

Posted on July 09, 2014 at 13:17 Hi Guys, I'm trying to generate Interrupt on INT1 to allow LIS3DSH to wake up my uController in order to read and manipulate the data. the below code with Registers configuration was used but not luck so ...

wal99d by Associate II
  • 1914 Views
  • 3 replies
  • 0 kudos

SPI?

Posted on August 03, 2015 at 18:01I'm trying to talk to a LSM6D3 over PCI. Everything's connected according to the datasheet in mode 1 (3.3v to VDD and VDDIO, SCx and SDx tied to GND) . I'm starting slow, so here's clock (SPC) and chip select (CS):h...

lee23 by Associate II
  • 807 Views
  • 0 replies
  • 0 kudos

MP34DT01 R/L channel selection

Posted on August 03, 2015 at 07:46Can anybody tell me that Why Audio sensor requires R/L selection as audio sensing is omni directional. I agree for audio reception (e.g. headphones) it's right choice to have..

rucha by Associate
  • 641 Views
  • 0 replies
  • 0 kudos

STEVAL-MKI109V2 with STEVAL-MKI142V1 - I2C mode

Posted on July 29, 2015 at 17:05All:I have procurred a STEVAL-MKI109V2 and plug-in board STEVAL-MKI142V1 (LPS25H). When I bring up the UNICO ''Cross-platform User Interface for MEMS demonstration kits'', I am able to see that the device is operating...

tba10596 by Associate II
  • 1059 Views
  • 1 replies
  • 0 kudos

Accelerometer reading is always 0x00

Posted on July 31, 2015 at 02:16Hey I'm trying a new board, this is the stm32f411e-disco and I can't read acc. values, they are always 0x00 I've generated the project with STM32CubeMX V4.9.0 The config and the main code are below: &sharpinclude ''st...

0690X00000605TIQAY.png

Status on HTS221?

Posted on July 20, 2015 at 13:54Hi,We are developing a new sensor device where we are using the HTS221 sensor currently, the project is now in prototyping phase. Last week the HRS221 status was set to NRND on st.com, but this week the status is back...

LSM6 SPI

Posted on July 29, 2015 at 20:12I'm trying to talk to a LSM6D3 over PCI. Everything's connected according to the datasheet in mode 1 (3.3v to VDD and VDDIO, SCx and SDx tied to GND) . I'm starting slow, so here's clock (SPC) and chip select (CS):htt...

lee23 by Associate II
  • 883 Views
  • 0 replies
  • 0 kudos

Soft system reset on LSM9DS0?

Posted on April 09, 2015 at 01:12Since power cycle is not an option for my application, I'm curious if there's a way to do a soft system reset ('reboot') to the lsm9ds1 module? #lsm9ds0

gto by Associate
  • 1191 Views
  • 1 replies
  • 0 kudos

LSM9DS0 axis orientation and readings

Posted on August 24, 2014 at 10:44Hi, I'm trying to understand the readings I got for a LSM9DS0 on my board. If I hold the board on my desk, according to the datasheet I should read a negative value for the Z-AXIS, because Z-AXIS vector points up,  ...

LPS25H power consumption

Posted on June 16, 2015 at 08:38Hi, I use LPS25H in my project. Based on the application note AN4450 page 13,(example 1) when I configure the LPS25H to the mode that ODR is 25 Hz,  pressure average 512, temperature average 64 (register 0x20 is 0xC0,...

hitwch by Associate II
  • 1076 Views
  • 1 replies
  • 0 kudos