cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-MKI109V2 with STEVAL-MKI142V1 - I2C mode

tba10596
Associate II
Posted on July 29, 2015 at 17:05

All:

I have procurred a STEVAL-MKI109V2 and plug-in board STEVAL-MKI142V1 (LPS25H). 

When I bring up the UNICO ''Cross-platform User Interface for MEMS demonstration kits'', I am able to see that the device is operating, and it has good values. However, can the interface be changed from the default SPI to run as I2C?

I would like to do this to evaluate a target board that has been made up with an I2C interface.

I realize that I2C may not be an option for the demo, but is it an option?

If so, how do I change the UNICO settings to use the I2C option?

Regards,

Todd Anderson

#unico
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
licciardello.anto
Associate II
Posted on July 31, 2015 at 10:43

Hi Todd,

I'm sorry. It is no possible change the UNICO settings to use the I2C option.

Regards

Antonella

All:

I have procurred a STEVAL-MKI109V2 and plug-in board STEVAL-MKI142V1 (LPS25H). 

When I bring up the UNICO ''Cross-platform User Interface for MEMS demonstration kits'', I am able to see that the device is operating, and it has good values. However, can the interface be changed from the default SPI to run as I2C?

I would like to do this to evaluate a target board that has been made up with an I2C interface.

I realize that I2C may not be an option for the demo, but is it an option?

If so, how do I change the UNICO settings to use the I2C option?

Regards,

Todd Anderson