MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DSH State Machine ?

Posted on March 08, 2016 at 10:56 Hello ,everyone. Now, I have some prolem about LIS3DSH . I tried run ''state machine'' LIS3DSH presets WakeUp from AN3393 page 78, but anything I do, the interrupt occur on INT1 all the time. What is the Probl...

stc3105 convert data

Posted on March 07, 2016 at 01:04Hey. I understand that this topic is not the place, there was no forum for the addition.Help with data conversion, we need the full formula. For example, at current consumption register REG_CURRENT is 65527, as I und...

den2life by Associate II
  • 991 Views
  • 1 replies
  • 0 kudos

Detecting accelerometer orientation (LIS2DH12)

Posted on March 03, 2016 at 18:02I am using the LIS2DH12 chip in a small battery powered box in users' vehicles. Whenever a user accelerates the vehicle, I would like to find out if the vehicle is moving forwards, or backwards, or turning, or going ...

yogesh by Associate
  • 888 Views
  • 0 replies
  • 0 kudos

ST LSM6DSL or Invensense MPU-6555 ?

Posted on March 02, 2016 at 18:42Hi, we have to chose a accelerometer/gyro combo for our sleep/motion tracking wearable. We have a big focus on energy consumption since the form factor of our wearable device should be exceptionally small and therefo...

LPS25H pressure range?

Posted on February 19, 2016 at 17:26Greetings. I would like to use the LPS25H/B as a pressure measuring device up to ~15 psi ''differential''. I know that the datasheet lists the functional range from 260 to 1260hPa absolute, how does this translate...

cphelan by Associate II
  • 1810 Views
  • 3 replies
  • 0 kudos

Read From i2c interface

Posted on February 25, 2016 at 16:11Hi everyone,I'm new user of ST product and i want to know if i can use inemo-m1 as a slave device to read datas from sensors.Thanks for reading and help.Salim

salim by Associate II
  • 686 Views
  • 0 replies
  • 0 kudos

HTS211 with different IIC address

Posted on February 24, 2016 at 07:01Hi, we need a humidity sensor for IoT home application systems. HTS211 looks very nice as it seems to be I2C readable at any time (whereas other sensors often need a complicated Measure-Pause-Read Intervall timing...

flyer31 by Senior
  • 1139 Views
  • 3 replies
  • 0 kudos

LPS22HB calibration

Posted on February 11, 2016 at 23:52I am looking to increase the absolute accuracy of the LPS22 pressure reading.  It appears OPC can be set using registers 18h and 19h after soldering.  Can this give my an absolute altitude reading (at a small defi...

cgeisz by Associate
  • 1547 Views
  • 1 replies
  • 0 kudos

Use LIS2HH on the same SPI bus with EEPROM, is it possible?

Posted on February 19, 2016 at 09:40I'm planning to use a LIS2HH on the same SPI bus as an EEPROM. But in the datasheet it says the LIS3DH CS pin is selecting SPI or I2C.So is it possible to use SPI to the EEPROM when LIS3DH CS pin is high (the LIS3...

shriharsh by Associate II
  • 1156 Views
  • 1 replies
  • 0 kudos

Self test fail

Posted on February 17, 2016 at 14:36We have a LIS3DH accelerometer that have ended up in a latch-up state. The output data is -205/-1149/-4759 (X/Y/Z in mg). When performing the self test, the absolute difference between the 2 samples are 7/6/3 (X/Y...