MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS25HB Temperature Compensation Behavior

Posted on May 09, 2016 at 19:52My colleagues and I are evaluating the LPS25HB and came across some behavior we don't understand. There are two issues we are trying to resolve right now: Embedded temperature compensation behavior is confusing.Accur...

kris2 by Associate
  • 2703 Views
  • 4 replies
  • 0 kudos

Datalogger Application for Non Motion Sensors

Posted on June 15, 2016 at 12:24There is a utility for MEMS data logging in the Nucleo Packages but is there any Utility for datalogging Other sensors like UV Sensors and Mems MicroPhone Sensors?Eagerly waiting to know on this? #mems-microphone-a...

darla14 by Senior
  • 674 Views
  • 1 replies
  • 0 kudos

hts221 SPI driver

Posted on June 05, 2016 at 03:20hi, I'm using the HTS221 humidity and temperature sensor along with the STM32F205. They are connected over the SPI bus but I am unable to get the STM32F205's SPI communications working correctly. Can anyone recommend ...

doug2399 by Associate
  • 975 Views
  • 1 replies
  • 0 kudos

ST Motion Sensor

Posted on June 14, 2016 at 20:48Hello. I am designing a smartwatch prototype and recently purchased the MKI159V1 which has the LSM9DS1. My company is still under construction. I noticed I am having a little trouble finding the link for the software ...

jigle004 by Associate
  • 671 Views
  • 0 replies
  • 0 kudos

VL6180x working environments

Posted on June 13, 2016 at 17:33Can the VL6180x sensor work perfectly fine in both indoor and outdoor environments? Does the amount of light present in the environment affect the operation of the time of flight sensor? 

Proximity output state

Posted on May 26, 2016 at 21:00I would like to use VL6180X more like a conventional proximity sensor where an output pin is active a target is within range, and the output is inactive when the target is outside the specified range. I don't see a way...

LPS22HB Low current and low low noise mode?

Posted on May 20, 2016 at 16:19Hi, I'm alitle confused when reading LPS22HB datasheet. Can anyone tell me what are the differences between low-current and low-noise mode?I know that LPS22HB operates in 3 modes (for collecting data): one-shot mode, c...

le by Associate II
  • 3043 Views
  • 9 replies
  • 0 kudos