User Activity

Can somebody recommend an O-ring for the LPS33HW?Supplier, vendor, part number? Any of those would be helpful.Specifications for the O-ring are in DT0096, 1.15mm inner diameter, 1.0mm thickness.
Posted on February 07, 2018 at 21:32The 32L496G-Disco board I have is MB1260B, it is clearly not the board depicted on page 15 of MB1261.pdf. I assume the diagram is the Rev A board.
Posted on September 26, 2017 at 22:21My STM32L496G-Discovery shows up as an 'Unknown Device' in the Windows 7 Device manager.I tried connecting to it with the ST-LINK Utility, it gives a 'No ST_LINK detected' error message.Is there a way to directly...
Posted on July 07, 2017 at 19:35I'm trying to implement a FreeRTOS program on an STM32F429I-Disco (first rev.) using the examples in STM32CubeF4 (V1.16.0). Neither the 'Demonstration' project not the 'FreeRTOS_ThreadCreation' project will run. They ...
Posted on May 26, 2016 at 21:00I would like to use VL6180X more like a conventional proximity sensor where an output pin is active a target is within range, and the output is inactive when the target is outside the specified range. I don't see a way...