MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Linux Drivers for lsm9ds1

Posted on April 03, 2017 at 15:47Hi ST Experts,Currently i am working on lsm9ds1 sensor. We are done with hardware connection and we have tested it using sample application using ioctl. In this we are using the polling mechanism. We have to get data...

i didn't obtain licence key to enable the libraries

Posted on April 03, 2017 at 14:25i generated the keys with the OSXLicence wizzard and generated a mail to transmit information ('between lines') and with the nucleo f401re but i did n't received acknowledgement mail.Can you check this , i'll use it ...

STEVAL-IDB007V1, old usb serial fw detected, OLD DTM FW detected

Posted on April 02, 2017 at 12:47Hi All,I am using STEVAL -IDB007V1 development KIT, i installed BlueNRG GI c2.2.2, when i try to connect to the device(click connect), i am getting 2 messages:1-  old usb serial fw detected.2- OLD DTM FW fw detected....

Nav Dev by Associate II
  • 638 Views
  • 0 replies
  • 0 kudos

53L0-SATEL problem

Posted on March 23, 2017 at 13:25I'm having some troubles using the VL53L0X sensor (53L0-SATEL-I1 board); I used the other satellite board included in the x-nucleo-53L0A1 without any problems, but the 53L0-SATEL-I1 isn't working properly; it seems t...

LSM9DS DEN_A/G

Posted on March 29, 2017 at 18:10Hello,How could I enable the DEN_A/G signal?I succeeded to enable the DRDY_M or INT1_A/G signal but I have nothing on this DEN_A/G.Do you have any suggestion?Best regardsMich

Mich1 by Associate III
  • 1068 Views
  • 4 replies
  • 0 kudos

LSM303AGR how to get 12-bit resolution on accelerometer

Posted on March 28, 2017 at 20:03LSM303AGR how to enable high resolution mode on the accelerometer? I have done exactly as described in the data sheet/manual setting the LPen bit to 0 and the HR bit to 1. I can play around with these bits but it doe...

STEVAL-STLKT01V1 to command a motor

Posted on March 27, 2017 at 18:19Hello, I am currently working on the STEVAL-STLKT01V1 development kit and I would like to use the sensortile to give an analog output in order to activate a motor. Does anyone know which of the output pins of either ...

VL53L0X freeze after ~1 min of use

Posted on March 21, 2017 at 23:05Hello,I am trying to operate the VL53L0X through ADLINK I2C SEMA3.5R7 (com express) interface.I initialized all the registers correctly according to - https://github.com/pololu/vl53l0x-arduino/blob/master/VL53L0X.cpp...