cancel
Showing results for 
Search instead for 
Did you mean: 

Any issues using LIS3DH direct from coin cell unregulated power?

duppy
Associate
Posted on March 16, 2016 at 17:15

The LIS3DH works from 1.8V to 3.6V.

If I use it direct from a CR2032 coin cell w/o regulator, will there be any side effects as the voltage drops from 3.3V to ~2.2V?

For example, will the calibration drift substantially?

Is the drift something that I can adjust for in FW?

If other devices on the same VCC cause the VCC to drop 0.1V to 0.2V over ~ millisecond (but still > 1.8V) , can this cause false triggers on the LIS3DH?

I am not using the ADC, only the accelerometer.

Thanks

#lis3dh #accelerometer #cr2032
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0