cancel
Showing results for 
Search instead for 
Did you mean: 

About LSM330 Register Problem

leo2010
Associate
Posted on February 26, 2014 at 03:15

Currently, I am now using LSM330, the only reference driver I found is official Linux-OS driver. Since there's no programming guides, I search website for source code for reference, only to find that all source code I found have a different register definition.

For instance, in a project in github, among the initialization code block, the author wrote the code below:

    

this

->

setAccelSensitivity

(

accelSensitivity

);

    

    

// Check the datasheet (p29)

    

// Normal (1.344 kHz) / low-power mode (5.376 kHz) data rate

    

// Normal mode selected (default)

    

// x,y,z axis enabled (default)

    

writeRegister

(

chipSelectAccel

,

CTRL_REG1

,

0

b10010111

);

    

// High-pass filter mode selection : Normal mode (reset reading HP_RESET_FILTER) (default)

    

// High-pass filter cutoff frequency selection

    

// Filtered data selection : internal filter bypassed (default)

    

// High-pass filter enabled for CLICK function : filter bypassed

    

// High-pass filter enabled for AOI function on interrupt 2 : filter bypassed

    

// High-pass filter enabled for AOI function on interrupt 1 : filter bypassed

    

writeRegister

(

chipSelectAccel

,

CTRL_REG2

,

0

b00000000

);

With the definition below:

/***************************************************

LSM330 Registers for gyro and accelerometer

****************************************************/

#define WHO_AM_I 0x0F

#define CTRL_REG1 0x20

#define CTRL_REG2 0x21

#define CTRL_REG3 0x22

#define CTRL_REG4 0x23

#define CTRL_REG5 0x24

#define CTRL_REG6 0x25

#define REFERENCE_A 0x26

#define REFERENCE 0x25

#define OUT_TEMP 0x26

#define STATUS_REG 0x27

#define OUT_X_L 0x28

#define OUT_X_H 0x29

#define OUT_Y_L 0x2A

#define OUT_Y_H 0x2B

#define OUT_Z_L 0x2C

#define OUT_Z_H 0x2D

#define FIFO_CTRL_REG 0x2E

#define FIFO_SRC_REG 0x2F

#define INT1_CFG 0x30

#define INT1_SRC 0x31

#define INT1_TSH_XH 0x32

#define INT1_TSH_XL 0x33

#define INT1_TSH_YH 0x34

#define INT1_TSH_YL 0x35

#define INT1_TSH_ZH 0x36

#define INT1_TSH_ZL 0x37

#define INT1_DURATION 0x38

However, in LSM330 official datasheet, the accelerate motion sensor has no CTRL_REG1, and from the content, we can see that the author disable HPF for ACCEL, where's ACCEL-HPF??? Only gyroscope has two LPF and one HPF.

Anyone please help me understand this? Thanks very much. 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ali ergin gursoy
Associate II
Posted on December 13, 2016 at 15:52

Hi Wancheng,

I have trouble to read data from LSM330TR too. Have you found anything to solve the problem?