MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to reset FTH flag when put threshold on the LSM6DS3H

Posted on September 24, 2017 at 09:45We have a problem when use full fifo flag and when interrupt happend and we read FIFO flag FTH clears and process start again. When set interrupt on threshold of the FIFO and it happens when read that part of FIF...

darko23 by Associate
  • 678 Views
  • 0 replies
  • 0 kudos

Resolved! Unstable I2C Connection to STEVAL-MKI137V1

Posted on September 15, 2017 at 10:26Hi all,I connected STEVAL-MKI137V1 (Magnometer sensor) to STM32L152D-EVAL through I2C. The library I am using is from STM32CubeExpansion_MEMS1_V4.0.0.I connected I2C pins to PB11 and PB10 without any external res...

Resolved! LIS2DH incorrect I2C address?

Posted on September 21, 2017 at 23:49Hi all,today I started a new project using the LIS2DH accelerometer (I2C mode). Previously I already used, very successfully, LIS3DH, always in I2C mode. Seeing the datasheets, in the basic functionatity, LIS2DH ...

MP34DT01 noise issue

Posted on September 21, 2017 at 11:59I'm using MP34DT01 MIC ,but i found that the niose is extremely large.My mcu is STM32F429VGT6,using its I2S peripheral.I use  libPDMFilter_IAR library convert  PDM signal to PCM signal.but there is a large amount...

VL6180X API and sample code

Posted on April 26, 2017 at 11:02Hello, I am using VL6180X-SATEL on STM42F4 Discovey Board and download the STSW-IMG003 software. When I implement it in Keil v5.0.0 and try to use vl6180x_simple_ranging.c code, program shows mi 3 errors, that file v...

LPS25HB unexpected behavior when FIFO is active

Posted on July 07, 2016 at 13:26I've encountered a problem with LPS25HB. I'm trying to get maximum precision from this barometer sensor without taking into account power consumption. I've setted up registers in this way and in this order: CTRL_REG1 ...

0690X0000060MnfQAE.gif

LPS25HB FITs and Reliability data

Posted on September 13, 2017 at 11:50Hi,I am looking for the FIT data and test conditions for part number LPS25HB. I could not find the information available on the website.

Accelerometer and Respiration

Posted on September 12, 2017 at 12:16Hi, everyone,I am quite a newbie in MEMS sensors!Just got a sensor Tile at hand, having fun with this device and the app.I am wondering if someone uses 3D accelerometers like LIS3DH to measure the respiration rat...

0690X00000602RJQAY.bmp
Zt Liu by Senior III
  • 1178 Views
  • 3 replies
  • 0 kudos

Resolved! H3LiS331DL : Noise of about +/-10g in all the axis and Z axis data is always offset by a value of about +8g.

Posted on August 26, 2017 at 11:40I am reading data through I2C. The calculations performed are correct (Converting high and low bytes into a 12 bit value and using 195mg/digit to convert data into scales of +/- 400g level.).There is a noise of abou...