MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL6180X operation

Posted on March 01, 2016 at 17:10I undesratnd that ''ST Time of Flight technology uses photon detectors to measure the time it takes a generated light pulse to leave our product, then reflect from a target and come back to our device.  Knowing the t...

VL53L0x ambient light sensitivity

Posted on August 03, 2017 at 10:30HiI am testing the VL53L0X time-of-flight sensor, in order to find out how resistant it is to ambient light and it turns out that if you point a light source with a high IR content (like a halogen light bulb) toward...

Optical issues for use of VL53L0X ToF sensor

Posted on December 01, 2017 at 09:38I would like to use the VL53L0X to determine the position of a linear position actuator (i.e., a device long and thin relative to its width).  Therefore, I would like to restrict the effective field of view of the...

How to decrease the VL53L0X FOV?

Posted on October 23, 2017 at 16:13Hello.Does anybody knows if is possible to decrease the VL53L0X FOV putting in front of It a short piece of plastic (dark?) pipe?Could it works enough fine or the cross-talk will become unacceptable?Any other optio...

Measuring VL6180X with close distances

Posted on August 16, 2017 at 16:36Hey,I am having the VL6180X Satellites sensor for ranging measurements. After connecting it, I receive some measurement values - but they are the wrong ones. The sensor isn't reacting to changes in a distance betwee...

Suggestion for compass

Posted on January 02, 2018 at 13:02Hi. Happy new year !I'd like to use one of ST compass + accelerometer chip (2 in 1) for implementing with one of analog device gyroscope in Kalman filter. Which sensor do you offer?  what is the criteria of choosin...

joe ted by Associate II
  • 983 Views
  • 1 replies
  • 0 kudos

vl53l0x I2C tBUF min=1.3ms?

Posted on November 30, 2017 at 16:48We've noticed that the datasheet states the following about I2C timings:tBUF - Bus free time between transmissions must be minimum 1.3msFor a 400kHZ I2C transmission, that sounds quite a long wait between frames.....

j i by Associate
  • 876 Views
  • 1 replies
  • 0 kudos

VL53L0X, 2mA current consumption when GPIO1 - INTERRUPT is configured

Posted on November 30, 2017 at 16:39Hi.We have integrated a VL53L0X TOF sensor, and we are getting very surprised when measuring current consumption.In the datasheet there is no mention to current consumption when GPIO1 is configured to interrupt.We...

j i by Associate
  • 1006 Views
  • 1 replies
  • 0 kudos

STM32 and VL53L0X

Posted on December 09, 2017 at 19:30Hey there,I'm working with my STM32L476 and the VL53L0X rangngs sensor.I'm using the Example from X-CUBE-53L0A1. I don't have the Nucleo board for the Sensor just a satellite board.  When using the example for ran...

Jonas L by Associate
  • 2264 Views
  • 3 replies
  • 0 kudos

Have problem with the HTS211 sensor

Posted on January 01, 2018 at 04:43Hi everyone!When i  send the 0xBE to the HTS211 with I2C, but there is no the ACK from the sensor , the I2C picture just like this.what is the matter?

0690X00000609IYQAY.png