MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

H3LIS331DL

Posted on January 08, 2018 at 15:19Dear Team,I am trying to configure CTRL_REG4 of H3LIS331DL chip register value multiple times with default configuration, which is creating a problem of not generating data ready interrupt. If I am not configuring ...

aci_gap_start_general_discovery_proc

Posted on January 05, 2018 at 18:23I have just downloaded and using the 'STM32CubeFunctionPack_BLESTAR1_V1.4.0'.What I had noticed is, after calling aci_gap_start_general_discovery_proc() would take ~10 seconds forGAP_Start_General_Discovery_CB() be...

LIS2DE12 query related to #INT pins.

Posted on December 23, 2017 at 05:47Hello,I am using LIS2DE12 Accelerometer in my device interfaced with 32 bit STM32L4 sereis.Looking into the datasheet LIS2DE12 having two INT pins.My question is do i need to interface both pins with micro control...

LIS2DE12

Posted on January 04, 2018 at 08:44I am interfacing sensor with Micro controller and controller is working at +3.3V.VDD_IO and VDD are two power supply pins in sensor.If i am giving common supply +3.3V of controller to VDD_IO and VDD , will it work?...

IIS2DH Raw data to convert into G unit

Posted on December 29, 2017 at 04:40How I convert accelerometer X, Y and Z axis raw data into the unit of G. Can someone provide me the which equation I have to apply on the raw data so I can get the results in G unit. Moreover, how we calculate rol...

VL6180X Range Offset Change issue

Posted on February 01, 2017 at 09:47Hi, allI'm using some VL6180X devices on my custom board.Then, their range offset seem to change every start up about �5mm, although I adjust the offset as directed in application note.What affects the range offse...

ishikawa by Associate II
  • 2000 Views
  • 4 replies
  • 0 kudos

VL53L0X Close range

Posted on January 06, 2017 at 08:53Hi, I want to use VL53L0X for an application that will detect objects in close range, as close as possible in the order of a few cm.How to configure the sensor to get maximum performance at close range using the AP...