MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSL zero-g level offset accuracy

Posted on January 04, 2018 at 16:28Hi everyone,I'm using the lsm6dsl for acceleration measurement. But I'm getting big stationary offsets and I was wondering is that normal? Here are measurements from 5 different boards and all of them were carefull...

palenkic by Associate II
  • 3215 Views
  • 5 replies
  • 0 kudos

MTBF/FIT rate

Posted on January 12, 2018 at 07:51I need the MTBF/FIT rate for part number STMPE811QTR. Thank you.

LIS2DH: Minimum delay between commands during Self-test

Posted on March 28, 2017 at 17:08Hi,is it possible to know the minimum delay required to wait between register writing during the self-test?I write down my code, to make myself more clearwhile(1) { BYTE xH = 0; BYTE yH = 0; BYTE zH = 0; //HPF disab...

Cesco Gar by Associate II
  • 2209 Views
  • 3 replies
  • 0 kudos

Resolved! FIFO rounding details

Posted on December 15, 2017 at 20:25Hi, I'm working with a LSM6DSMTR device connected via I2C to a Nordic Semi nRF52382.  I would like to use the FIFO feature and have a question about the address rounding:If I start the multiple data read at the FI...

Resolved! Can X-CUBE-MEMS1 libraries be used in B-L475E-IOT01A board?

Posted on January 09, 2018 at 15:53I have a http://www.st.com/en/evaluation-tools/b-l475e-iot01a.html, which I am using now to learn about how ST MEMS sensors work and if I can use them in my future PCB designs.I have found recently that ST provides...

H3LIS331DL Accel Sensor turn-on Time Based on ODR

Posted on January 10, 2018 at 13:04Dear Team,In H3LIS331DL Datasheet, Page number 18, Ton (Turn-on Time)  Test condition : ODR = 100Hz, Typ. 1/ODR+1msBy this I understood that if ODR is 100Hz then we need 11ms after Accel is turnon.Then what about o...

Resolved! IIS2DH current consumption

Posted on January 08, 2018 at 16:39Hello,I am using IIS2DH to work for my application. But the problem rises when I measure the current it is consuming. At 25Hz with 40ms INT2 duration and Low Power Enabled with all axis, I am observing a current a ...

lps22hb

Posted on January 10, 2018 at 06:33Hi,can i use 7 lps22hb on I2C bus?thanks,francesco

Nucleo-L152RE + CubeExpansion_MEMS1 + Keil error

Posted on January 10, 2018 at 00:28I'm trying to build an example project that comes with the 'STM32CubeExpansion_MEMS1_V4.2.0' using Keil. It shows the following error: startup_stm32l152xe.s: error: A1023E: File '..\..\..\..\..\..\..\Drivers\CMSIS\...