cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSL zero-g level offset accuracy

palenkic
Associate II
Posted on January 04, 2018 at 16:28

Hi everyone,

I'm using the lsm6dsl for acceleration measurement. But I'm getting big stationary offsets and I was wondering is that normal? 

Here are measurements from 5 different boards and all of them were carefully positioned to be exactly at the same place. 

xyz

-159-411110

-7-781037

86701100

10-981089

171221162

Is this normal operation? 

In datasheet Linear acceleration zero-g level offset accuracy is specified at ±40 mg (typ), but my measurements are as much as 6 times that.. Am I doing someting wrong? 

In the datasheet they say that sensors are all factory calibrated before they go out of factory, but I do not see any register or anything with calibration values. Only ones for user calibration.

I hope my message was clear, sorry for my English.

Thanks

Martin

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Miroslav BATEK
ST Employee
Posted on January 04, 2018 at 19:52

Hmm, it is not normal operation. Can you please share your sensor configuration, schematic would be also usefull if it is posible to share.

The sensor are factory calibrated, but the calibration values are no accessible for user.

Miroslav BATEK
ST Employee
Posted on January 05, 2018 at 13:33

The schematics is OK and the code seems good as well.

The problem could be in the layout. Did you design the boards by yourself? Don't you have tracks of vias under the sensor?

One more question, are the values mentioned above stable or is there some significant noise.

Posted on January 05, 2018 at 14:34

Yes I did. There is ground polygon under the sensor as you can see from photos in attachment. A line on the bottom side (close to pins) is for a buzzer but it was not powered at the time of reading accelerator data.

Readout is pretty stable. Sometimes the values change by +/- 1 but that is it. It just has that big static offset.

________________

Attachments :

pcb-top side.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyDU&d=%2Fa%2F0X0000000b4l%2F3yPXRuCAX.BMgrE3hSO4eU_dUOcLoNVbykL7.UOPHL8&asPdf=false

pcb-top layer only.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyCD&d=%2Fa%2F0X0000000b4j%2F0278C4wIyAmc_lpF4M94ErpA5iR9RtxySqTNglGSLy0&asPdf=false
Posted on January 12, 2018 at 13:55

The layout is not fully adherent to ST recommendations (please check the

http://www.st.com/content/ccc/resource/technical/document/technical_note/73/17/9c/16/dd/96/4a/01/CD00134799.pdf/files/CD00134799.pdf/jcr:content/translations/en.CD00134799.pdf

) and it can introduce some additional offset.

I see mainly the problem with not symmetrical design.

You can use out MotionAC library to calibrate the accelerometer and reduce the offset by software. The MotionAC library is aprt of

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-mems1.html

package.