cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-L152RE + CubeExpansion_MEMS1 + Keil error

Soham Jani
Associate II
Posted on January 10, 2018 at 00:28

I'm trying to build an example project that comes with the 'STM32CubeExpansion_MEMS1_V4.2.0' using Keil. 

It shows the following error: 

startup_stm32l152xe.s: error: A1023E: File '..\..\..\..\..\..\..\Drivers\CMSIS\Device\ST\STM32L1xx\Source\Templates\arm\startup_stm32l152xe.s' could not be opened: No such file or directory 

I'm using X-NUCLEO-IKSO1A1 expansion board. 

Other examples that come with STM32Cube library build and flash fine. (Eg Blnky)

Would love some help figuring this out. Thanks 

#x-cube-mems1 #iks01a1 #nucleo-l152re
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0