MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interrupt status on VL6180X in interleaved mode

Posted on September 14, 2017 at 21:46Hi guys, I'm developing a application that uses a XNUCLEO-6180XA1. The development board is a PSoC-4 enabled board with arduino headers (http://www.cypress.com/documentation/development-kitsboards/cy8ckit-042-pso...

Resolved! Sensitivity of LIS3MDL (LSB/Gauss)

Posted on September 23, 2017 at 05:45I am using LIS3MDL sensor and I do not understand the sensitivity which its unit is LSB/Gauss.  In x-cube-mems1 library, the following is calculated:&sharpdefine LIS3MDL_MAG_SENSITIVITY_FOR_FS_4G    0.14 /**< Sen...

0690X00000603jKQAQ.jpg

How to reset FTH flag when put threshold on the LSM6DS3H

Posted on September 24, 2017 at 09:45We have a problem when use full fifo flag and when interrupt happend and we read FIFO flag FTH clears and process start again. When set interrupt on threshold of the FIFO and it happens when read that part of FIF...

darko23 by Associate
  • 449 Views
  • 0 replies
  • 0 kudos

Resolved! Unstable I2C Connection to STEVAL-MKI137V1

Posted on September 15, 2017 at 10:26Hi all,I connected STEVAL-MKI137V1 (Magnometer sensor) to STM32L152D-EVAL through I2C. The library I am using is from STM32CubeExpansion_MEMS1_V4.0.0.I connected I2C pins to PB11 and PB10 without any external res...

Resolved! LIS2DH incorrect I2C address?

Posted on September 21, 2017 at 23:49Hi all,today I started a new project using the LIS2DH accelerometer (I2C mode). Previously I already used, very successfully, LIS3DH, always in I2C mode. Seeing the datasheets, in the basic functionatity, LIS2DH ...

MP34DT01 noise issue

Posted on September 21, 2017 at 11:59I'm using MP34DT01 MIC ,but i found that the niose is extremely large.My mcu is STM32F429VGT6,using its I2S peripheral.I use  libPDMFilter_IAR library convert  PDM signal to PCM signal.but there is a large amount...

VL6180X API and sample code

Posted on April 26, 2017 at 11:02Hello, I am using VL6180X-SATEL on STM42F4 Discovey Board and download the STSW-IMG003 software. When I implement it in Keil v5.0.0 and try to use vl6180x_simple_ranging.c code, program shows mi 3 errors, that file v...