MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS22HB is giving same value

Posted on January 22, 2018 at 09:27Hi I am using  LPS22HB with my custom made board based on STM32F777. I am reading LPS22HB using the same driver as ST is giving. I always read the same value of pressure i.e 1847. Temperature value is also incorrec...

Queru on LIS3DH sensor

Posted on January 24, 2018 at 09:54Hi,I am working on LIS3DH accelerometer sensor, I have interfaced this sensor with STM32F103 series micro controller using SPI interface. When I read X, Y and Z acceleration values, I get some random readings and i...

IIS2DH capacitors to VDD line

Posted on January 28, 2018 at 00:34Hello,Is it mandatory that 100nF and 10uF to the VDD line has to be ceramic and aluminium respectively?Also, we had three custom boards built with IIS2DH. Surprisingly, all three were giving a different XYZ values ...

Why is my INT1 of LIS2DW always at high?

Posted on January 25, 2018 at 18:52Hi,    My problem is I can not receive the interrupt signal of INT1 when I using FIFO mode with FIFO buffer full trigger. I find the cause is that the INT1 is always at high, but I expect it should be rise high whe...

0690X00000609UdQAI.png 0690X00000609UiQAI.png
Allen Lin by Associate II
  • 1250 Views
  • 1 replies
  • 0 kudos

LSM6DS3 Accel-Gyro Data problem

Posted on January 25, 2018 at 11:16Hi, i am using this sensor for a while now ,and i have a problem when i use together accelerometer and gyroscope. When i use them seperately everything works great, but if use both of them and acquire data from the...

Alex Dim by Associate II
  • 902 Views
  • 0 replies
  • 1 kudos

Data mismatching while Hard and soft reset

Posted on January 18, 2018 at 06:19Hello Miroslav, I have done following configuration for IIS2DH acceleromenter./////////////////////////// Sample Code ////////////////////////////////////////////////////response=LIS3DH_GetWHO_AM_I(&who_am_i); if(w...

Bluecoin microphone distances

Posted on January 24, 2018 at 11:39Hello,I have 2 questions about the microphone distance of the Bluecoin hardware.I have ordered this hardware to experiment with the microphones and the beam-forming algorithms and it works very impressive. I would ...

Marcel . by Associate
  • 787 Views
  • 0 replies
  • 0 kudos

LIS2DE12 Activity/Inactivity detection

Posted on January 22, 2018 at 17:39HelloI want to detect the movement for 10 min from an accelerometer LIS2DE12, I want to know if I can use the configuration of the interuption register or i must use a REal time counter Thanks

LSM9DS1 : How to validate IMU feature in Android

Posted on January 22, 2018 at 08:51Hi ,I am using LSM9ds1 in one of my project. The main reason for using this chip is,  it is THE one recommended for IMU feature, where all 3 sensors are in one chip.In Android 6.0 , I am getting all 3 sensors data ...