Hi, I just can see a flash of CubProgrammer when I double click its short-cut icon. I have re-installed it several times. It always can give me a flash. My OS is windows 10 and JAVA version is JRE 8. The java environment setting is Path: C:\Prog...
Posted on March 12, 2018 at 14:48Hi, Thank you for reading my question. I always get the same values of x,y and z for using FIFO mode on LIS2DH12. The x, y and z values will change for each interrupt of WTM, but the three values are the same. M...
Posted on January 25, 2018 at 18:52Hi, My problem is I can not receive the interrupt signal of INT1 when I using FIFO mode with FIFO buffer full trigger. I find the cause is that the INT1 is always at high, but I expect it should be rise high whe...
Hi All, I find the root cause. It installs at JKD 11 when I install CubeProgrammer first time. But It still installs at JDK 11 after I install JRE 8 and set the path and JAVA_HOME for JRE8. It works well after I remove JDK11