MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH as movement/tilt sensor

Posted on February 05, 2018 at 19:54Hi ALL, I bought the LIS3DH development kit.I want to use it as a sensor that will wake my MCU with interrupt when someone moved my board or tilt it.I have some constrains:1. I need low consumption current with my...

Id At by Associate II
  • 4014 Views
  • 10 replies
  • 0 kudos

LSM303AGR Low ESR capacitor

Posted on February 09, 2018 at 10:31Hello, in the LSM303AGR datasheet a low esr capcitor (220nF) is requested on pin5. But no more indication are given.On which frequency the esr must be < 200mOhm ?Thanks for the help.#lsm303agr

Recommended LIS2DH Setup

Posted on November 01, 2017 at 18:16I have an LIS2DH device in my design and it's working - sort of.  I was given some LIS3DH C driver code which I'm using under the advice that the LIS2DH is register-compatible with the LIS3DH.So my requirement is ...

LIS2DH self test & interrupt

Posted on February 06, 2018 at 09:55Hi,I am looking to test if the interrupt 1 and 2 are working correctly on a LIS2DH.Is it possible to trigger interrupts with the self test functon ?Thank you for the help#lis2dh #self-test #interrput

STPM10 does not start immediately after RC startup procedure

Posted on March 08, 2017 at 10:53Hello all,I want to use ♯ with internal RC oscillator. When I started using ♯ , I prepared a communication library that works well without using the internal RC oscillator. I checked all communication using oscillosc...

LPS22HB is returning zero as the sensor output

Posted on February 05, 2018 at 23:46After initializing an SPI 3-wire interface with a STM32L4 MCU on a custom board, the driver always returns zero as the pressure value whenever the get pressure method is called. Even the temperature sensor reading...

LPS25HB for force readings

Posted on February 02, 2018 at 12:08Dear all, I am inquiring the possibility to use LPS25HB absolute pressure sensors as force sensors. My idea is to integrate the sensors into a rubber or silicon layer (5 - 10 mm thick) so that the rubber layer, ac...