cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DH self test & interrupt

charles cordiez
Associate
Posted on February 06, 2018 at 09:55

Hi,

I am looking to test if the interrupt 1 and 2 are working correctly on a LIS2DH.

Is it possible to trigger interrupts with the self test functon ?

Thank you for the help

#lis2dh #self-test #interrput
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Miroslav BATEK
ST Employee
Posted on February 06, 2018 at 21:06

There is no built-in function to test interrupts.

But you can for example setup threshold interrupt to some very high value and set the condition to enable interrupt if measured acceleration is below the threshold, so this will artificaly trigger the interrupt without need to do a movement with the sensor.

M Poppitz
Associate II
Posted on February 08, 2018 at 23:41

actually you can self test the interrupts with the built in self test.

If you read the spec sheet look at sections 7.6 thru 7.9  

in CRTL_REG3  you need to set the I1_AOI1 and 

I1_AOI2 bits to 1 to activate the interrupts, by default they are 0.

Weather in self test mode or using external vibration to test, these will activate the interrupts based on the preset threshold levels.

You simply have to determine what levels you want to use if using vibration to test, in self test mode the interrupts should fire.

One of the easiest is of course attach the LIS2DH int pins to interrupts on the micro to see if they fired.