MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL6180X addressing multiple sensors

Posted on July 23, 2017 at 16:03I am working with the VL6180x and I would like to connect multiple sensors via an expansion board by ST (*). Therefore I want to communicate to single sensors, so I have to change each single I2C-Device-Address via th...

STEVAL-WESU 1 Accelerometer reports 0 data

Posted on August 16, 2017 at 11:52The accelerometer on my STEVAL-WESU1 has stopped reporting data. For instance, in the Plot data demo, I can see:Data: X: 0  Y: 0  Z: 0After I charge it, it does report some data but only for some seconds.I can see t...

STEVAL-WESU1 Accelerometer reports ''0'' data

Posted on August 16, 2017 at 11:44My STEVAL-WESU1 does not report any Accelerometer/Gyrometer data anymore.In the Plot data menu, I can see:Data: (X: 0 Y: 0 Z: 0)If I charge my STEVAL and start the demo, it will report data for some seconds, and the...

LIS2DE12 Interrupt configs, Offset correction and ...

Posted on August 15, 2017 at 23:13Hi,I'm trying to use LIS2DE12 for position recognition of device, but i faced some strange problems !1- I didn't find any solution to correct the offset values of X Y Z dimensions ! i.e after soldering the chip, whe...

6D orientation detection with LIS3DH

Posted on February 03, 2017 at 16:40Hi all,I'm using a LIS3DH accelerometer and I would like to detect the device orientation in the space. According to the specifications I could do this by means of the 6D orientation detection function, but I'm no...

Precision difference between LPS22HB and LPS25HB

Posted on October 29, 2016 at 12:25Hi, I can read from LPS25HB ST description page that it have ''High-resolution mode: 0.01 hPa RMS'' while on LPS22HB there's nothing about this. But looking at either datasheed I've found that: LPS22HB PAccT +/-0.1...

VL53L0X measurement profile/spec

Posted on June 30, 2017 at 22:32Hi,changing the timing budget affects the measurment accurancy/speed/range.  This is done with the function VL53L0_SetMeasurementTimingBudgetMicroSeconds(..). Does this function affects the measurements parameter in t...

dialogue by Associate
  • 691 Views
  • 2 replies
  • 0 kudos

LIS2HH12 Noise Information

Posted on August 16, 2016 at 17:37Hi, I've a design based on LIS344ALH where the noise level is a very sensitive parameter since I need to measure signals in the mg range. I would like to move to a full digital component and I'm looking to the LIS2H...

cn2 by Associate II
  • 1548 Views
  • 7 replies
  • 0 kudos

LIS3DH accelerometer sensitivity in low power mode

Posted on July 17, 2015 at 15:05Hello,I am planning to operate the LIS3DH accelerometer in low power mode (resulting in an output data rate of 5kHz according to Table 26 in the datasheet).In Table 3 in the datasheet a sensitivity of 12mg/digit is gi...

stephan by Associate
  • 1383 Views
  • 3 replies
  • 0 kudos

LIS3DH 5kHz ODR not possible

Posted on May 09, 2016 at 15:33Hello all, I want to use the LIS3DH accelerometer and a Steval-MK1109v2 Motherboard with the ST Unico GUI for logging Acceleration data. The datasheet of the LIS3DH shows the possibility to meassure a bandwidth up to ...